Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.
The following page content corresponds to the products formerly marketed by NEC Electronics
Presenting the World's First USB 3.0 Compatible LSI Host Controller
µPD720200 is the world's first USB 3.0 compatible LSI host controller that is compliant with USB 3.0, the next-generation standard of USB. The stress of transferring large amounts of data is eliminated through high-Speed data communication that is 10 times faster than existing products.
Product Lineup
| USB3.0 | |
|---|---|
| USB3.0 Host Controller |
|
| USB2.0 | |
| USB2.0 Host/Peripheral Controller |
|
| USB2.0 Host Controller |
|
| USB2.0 Hub Controller |
|
| USB2.0 IDE Bridge |
|
NEC Electronics prepare the microcontrollers with USB control function (host and peripheral).
Please refer to the "Microcontrollers" web page.