Beginning of this page
Jump to main content

Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.


The following page content corresponds to the products formerly marketed by NEC Electronics

SID Display Week 2008

NEC Electronics America will demonstrate a full suite of LCD modules at Display Week 2008.

Visit us in booth no. 235 to learn more about our complete solutions for medical, industrial and high-resolution display applications. Several technologies will be showcased:

  • White LED-Based Products
    NEC Electronics America will be exhibiting a variety of industrial-type LCDs with LED backlights, from small-size mobile LCDs to large-size high-resolution LCDs.

  • Displays with Wide Aspect Ratios
    for Industrial Uses

    A number of display modules with wide aspect ratios for industrial-type applications will be demonstrated in the NEC Electronics America booth. Displays range from a 4.1-inch WVGA LCD to a 22.5-inch WUXGA LCD.
SID Display Week 2008

  • Mobile Displays for Industrial Applications
    NEC Electronics America will showcase a variety of mobile LCD modules designed for industrial-type applications. The modules range in size from 2.7-inch to 4.3-inch. In addition, small-size QHD LCDs and a small 2D/3D display will be demonstrated.

View the SID 2008 media kit for recent display module press releases and the latest issue of the LCD Newsletter.




SID Display Week 2008
Los Angeles
Convention Center,
Los Angeles, California

Exhibit Dates/Times
Tuesday, May 20
10:30 a.m. to 5:00 p.m.

Wednesday, May 21
9 a.m. to 5:00 p.m.

Thursday, May 22
9 a.m. to 2 p.m.

Display Week 2008