Beginning of this page
Jump to main content

Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.


The following page content corresponds to the products formerly marketed by NEC Electronics

Glossary


Body-bias

Technology for reducing current leakage by varying the voltage applied to a circuit. The substrate or body of the circuit is connected to a bias voltage to control the transistor threshold. Standby current leakage can be reduced by applying a reverse bias.



Subthreshold leakage (ISUBTH)

The current that flows between the source and drain of a transistor when the transistor is in the off state.



High-k dielectric

A material with a high dielectric constant (k, a measure of how much charge a material can hold) compared to the silicon dioxide material used in semiconductor insulating layers. Because high-k gate insulating layers have higher permittivity than silicon dioxide, they are also called high permittivity layers. High-k dielectric materials can be used in physically thick insulating layers that reduce leakage current while having an electrical thickness comparable to a thin layers of silicon dioxide. NEC Electronics uses a highly reliable HfSiOx High-k dielectric material.



GIDL (Gate Induced Drain Leakage)

A current that leaks from the drain to the substrate of a transistor. In the transistor off state, GIDL currents arise in the high electric field under the gate/drain overlap region.