Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.
The following page content corresponds to the products formerly marketed by NEC Electronics
For speed and simplicity, NEC Electronics configures eDRAM read and write procedures to work like those of SRAM. On consecutive reads, writes and alternating read/write cycles, NEC Electronics eDRAM provides SRAM-like sequences that have no idle cycles. By eliminating the need for the complex commands associated with SDRAM, our eDRAM is easy to integrate into your SoC design.
Embedded DRAM must be refreshed periodically and refresh is the only restriction of eDRAM. The refresh scheme of NEC Electronics eDRAM is
row-only-refresh (ROR). One row must be either refreshed or accessed by read or write operation within the maximum data retention time (tREF). One clock cycle is required to refresh one row.