Beginning of this page
Jump to main content

Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.


The following page content corresponds to the products formerly marketed by NEC Electronics

PMD Applications


  • Third-Generation Mobile Phones
    NEC Electronics offers a lineup of MOSFETs that achieve low on-resistance by employing leading-edge process (0.25 µm) and wireless bonding implementation technologies.

  • Automotive Electronics
    World-class low on-resistance has been achieved by combining a UMOS4 0.25 µm process with leading-edge trench technology and new multibonding implementation technology to provide a variety of products suitable for a range of applications.

  • Flat Panel Televisions
    NEC Electronics offers a lineup of small packages from SOP8 to SC95, and will continue to supply new products to meet the latest market needs.

  • Set-Top Boxes
    NEC Electronics offers power MOSFETs for power supply blocks, and noise clipping diodes for high-speed serial communications.

  • Desktop Computers
    NEC Electronics offers a variety of small, low on-resistance power MOSFETs mounted on motherboards, as well as NSAD and NNCD Series ESD protection devices.

  • Notebook Computers
    NEC Electronics offers a variety of small, low on-resistance power MOSFETs mounted on motherboards, as well as NSAD and NNCD Series ESD protection devices.

  • Hard Disks
    NEC Electronics offers a lineup of MOSFET products suitable for hard disk power supplies, contributing to lower power consumption.

  • Digital Cameras
    The NSAD series with ESD protection, is suitable for use in USB 2.0 and IEEE 1394-compliant high-speed interfaces. Its low terminal capacitance allows ESD protection that does not affect high-speed data transfer.

  • Digital Camcorders
    NEC Electronics offers motor driver ICs for zooming or focusing and power MOSFET products for power supply blocks.

  • Onboard Power Supplies for Communications Devices