Beginning of this page
Jump to main content

Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.


The following page content corresponds to the products formerly marketed by NEC Electronics


View interface products.
View USB products.
View Wireless USB products.

NEC Electronics Expands Wireless USB Portfolio with New Host Controller

Higher Throughput, Higher Performance for Laptops

KAWASAKI, Japan, DUESSELDORF, Germany, SANTA CLARA, Calif. (U.S.A.), August 19, 2008 — NEC Electronics today expanded its suite of Wireless USB devices with the introduction of the uPD720171 Wireless USB host controller. Building on the company's first host controller (part number uPD720170), the new uPD720171 controller for PCI Express™ bus interfaces, enables high-speed, wireless data transmission between PCs that have MiniCard or Half-Minicard expansion cards and PC peripheral devices such as wireless hubs, printers, external storage equipment and digital cameras. The new host controller also provides laptop computer connectivity through an ExpressCard™ slot. Providing greater throughput and higher performance than previous host devices, the uPD720171 controller enables consumers to enjoy wireless lifestyles while maintaining wired USB functionality and ease of use.

"As the consumer appetite for wireless connectivity increases, the industry is requiring reliable, standardized interface solutions that can transmit data at speeds equivalent to wired USB connections," said Yoshiyuki Tomoda, Group Manager, SoC Systems Division, NEC Electronics Corporation. "By providing these performance levels, our new uPD720171 host controller is helping bring the industry closer to mainstream adoption of advanced wireless technologies."

Certified by the USB Implementers Forum (USB-IF), the uPD720171 controller conforms to the Wireless USB 1.0 specification and also to the Wireless Host Controller Interface (WHCI) specification developed by Intel with support from Microsoft, NEC Corporation, Philips, Texas Instruments and other experts in Wireless USB technology.

Capabilities of Wireless USB
Developed by the Wireless USB Promoter Group, Wireless USB technology builds upon the current USB 2.0 standard, which has been hailed as the next-generation interface standard for computers and multimedia consumer electronics devices. The Wireless USB specifications supports data transfer rates of up to 480 megabits per second (Mbps) of data, comparable to wired USB 2.0 connections at close range. NEC Electronics' new controller can transfer up to 480 Mbps within a maximum range of three meters.

Unwiring the cable connection frees users from having to make cumbersome and unsightly wired connections and enables them to enjoy high-speed data access using Wireless USB. Currently, Wireless USB technology is making it possible for designers to expand the boundaries of computing and digital entertainment to discover new ways for consumers to enjoy digital media.

NEC Electronics has played a central role in making the current USB 2.0 one of the most successful interfaces in the history of personal computing. NEC Electronics is a USB-IF board member, which manages the compliance and certification program, branding, marketing and industry education of USB and Wireless USB technologies. Since launching volume production of USB 2.0 devices in 2000, NEC Electronics has shipped an industry-leading 150 million units worldwide.

Pricing and Availability
Samples of NEC Electronics' uPD720171 Wireless USB host controller are available now at US$10.00 each (pricing and availability are subject to change). Reference boards are also available upon request. More information about NEC Electronics' lineup of Wireless USB solutions can be found at http://www.necel.com/cwusb/en/newproducts.html.

About NEC Electronics
NEC Electronics Corporation (TSE: 6723) specializes in semiconductor products encompassing advanced technology solutions for the high-end computing and broadband networking markets; system solutions for the mobile handset, PC peripheral, automotive and digital consumer markets; and multi-market solutions for a wide range of customer applications. NEC Electronics Corporation has subsidiaries worldwide including NEC Electronics America, Inc. and NEC Electronics (Europe) GmbH. More information about NEC Electronics worldwide can be found at http://www.necel.com.

# # #

NEC Electronics and NEC Electronics America are either registered trademarks or trademarks of NEC Corporation in the United States and/or other countries. All products and services mentioned in this release are trademarks or registered trademarks of their respective owners. ExpressCard is a trademark of PCMCIA in the United States and/or other countries. PCI Express is a registered trademark of PCI-SIG®.