Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.
The following page content corresponds to the products formerly marketed by NEC Electronics
The V850ES/Jx2 microcontrollers guarantee high-speed action during 3V operation, making them optimal for applications in digital home electronic systems that are increasing in complexity, multifunctionality, and speed.
The V850ES/Jx3 microcontrollers are equipped with a high-capacity memory of 1 MB. Naturally furnished with functional interchangeability and pin interchangeability with the V850ES/Jx2 microcontrollers and capable of appropriating their development environment as well, the V850ES/Jx3 devices are capable of realizing system acceleration with ease.
The newest arrival to the lineup is the V850ES/Jx3-L microcontroller, an ultra-low power-consuming version of the V850ES/JG2 microcontroller, with less than half of its power comsumption current. The V850ES/Jx3-L lineup has achieved an industry-leading nominal power/performance ratio (0.9 mW/MIPS, which comes in under the 1 mW marker according to the Dhrystone evaluation) and actual operating current of 13 mA typ. (at 20 MHz)