Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.
The following page content corresponds to the products formerly marketed by NEC Electronics
The ancestor of all of NEC Electronics' 32-bit microcontrollers is the original V850 core. Though once very popular, it is no longer used for new microcontroller designs since its successors, the V850ES and V850E1/E2 cores, are readily available.
The V850ES is optimized for lowest costs, making it an ideal choice for applications often served by 16-bit microcontrollers. To complement this, the V850E1 core was designed for high performance. Later, its successor, the V850E2, pushed the performance bar even further.
From the feature highlights in the table below, click an application link for more product information.
| |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||