Beginning of this page
Jump to main content

Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.


The following page content corresponds to the products formerly marketed by NEC Electronics

V850 (32-bit) Microcontrollers


NEC Electronics' V850™ microcontrollers incorporate a 32-bit RISC core based on Harvard architecture. Hence, the core hardware can be simplified and the core size minimized. As a result, our microcontrollers provide maximum performance at the lowest cost.


Product Linup for V850 Microcontrollers

V850E2/ME3 V850E/ME2 V850E/MA3 V850E/MA2 V850E/MA1 V850/SB2 V850/SC2 V850/SB1 V850/SC1 V850E/SV2 V850/SA1 V850/SA1 V850/SV1 V850ES/SA2 V850ES/SA3 V850ES/HE3 V850ES/HF3 V850ES/HG3 V850ES/HJ3 V850ES/HE2 V850ES/HF2 V850ES/HG2 V850ES/HJ2 V850ES/JG3 V850ES/JJ3 V850ES/JF3-L V850ES/JG3-L V850ES/JG2 V850ES/JJ2 V850ES/KE2 V850ES/KF2 V850ES/KG2 V850ES/KJ2