Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.
The following page content corresponds to the products formerly marketed by NEC Electronics
Reference Design with V850ES All Flash Microcontrollers
The AF-EV850 board serves as an evaluation board for the All Flash V850ES microcontroller lineup from NEC Electronics. The AF-EV850 board supports three devices, V850ES/KJ2, V850ES/HJ2 and V850ES/JJ2, each represents the superset device from the three sub-series of the All Flash lineup.
Note: either the MINICUBE for V850 or the MINICUBE2 is required with this board.