Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.
The following page content corresponds to the products formerly marketed by NEC Electronics
Complying with the latest-generation JEDEC standard for system memory, the µPD720900 Advanced Memory Buffer (AMB) works with SDRAM to implement high-capacity, high-throughput memory subsystems for applications such as servers and workstations. The µPD720900's SDRAM interface connects directly to DDR2-533, DDR2-667 and DDR2-800 devices. To support the JEDEC-standard, fully buffered DIMM (FB-DIMM), daisy-chained bus architecture, the µPD720900 provides FB-DIMM interfaces that enable 3.2-, 4.0- or 4.8-Gbps channel bit rates.
With these high-speed channels, the full-featured µPD720900 connects in a daisy chain with multiple AMB-based DIMMs and a host memory controller. As many as eight AMB devices can work seamlessly on each FB-DIMM channel, thus allowing use of very large memory capacities. The AMB smart interface accepts memory requests for its local DDR-2 SDRAM or forwards memory requests to other AMB-based DIMMs.
The µPD720900 AMB supports server, workstation, router and graphics controller applications with an industry-standard architecture that will become the mainstream server/workstation memory solution. These FB-DIMM memory subsystems offer reduced cost, greatly improved memory capacity and better signal integrity than existing stub-bus architectures. Designed to deliver on FB-DIMM's capabilities for extremely high reliability, the NEC Electronics µPD720900 AMB meets demanding application requirements for high-RAS (reliability/ availability/serviceability) systems.
Figure 1. µPD720900 Advanced Memory Buffer (AMB)