Beginning of this page
Jump to main content

Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.


The following page content corresponds to the products formerly marketed by NEC Electronics

U.S. Wafer Foundry Overview


TECHNOLOGY
Beyond our range of CMOS-fabricated semiconductor products from 0.15 to 0.35 µm, NEC Electronics America can implement customer-specified processes in 0.15 µm design rules or larger. 

COT DESIGN FLOW
With NEC Electronics' COT design flow, you can take advantage of more than just our world-class manufacturing facility. You will have access to options like an IP core library, test design and macro design services at the LSI design phase, and assembly and testing after fabrication, as well as other options listed under Design Services. 

DESIGN SERVICES
Our facility is not just world class. So are the people who work there. One of the most important benefits of working with the NEC Electronics America foundry in Roseville is the unprecedented access you'll have to our team of experienced production engineers, as well as our design engineers in Santa Clara, California. 

FACILITY
Working with NEC Electronics America helps you avoid the constraints that may have made manufacturing your chips difficult in the past. Our U.S. location means time and language are no longer barriers. You have the ability to work more closely with design, product, process and RQC engineers. 

CONTACT INFORMATION
To find out how NEC Electronics America can get your chips into production right away, please call 800-366-9782 or contact our foundry team




 

Press Releases

 
 
NEC Electronics America Inducted Into Environmental Protection Agency's WasteWise Hall of Fame (Mar 22, 2010)
 
 
NEC Electronics America to Close Its Six-Inch Wafer Fabrication Line by March 2010, Exclusively Focus on Eight-Inch Line (Jan 29, 2009)
 
 
NEC Electronics America Expands Capacity on New Eight-Inch Line at Wafer Fab in Roseville, California (Oct 06, 2008)
 
 
NEC Electronics and ELMOS to enter Strategic Partnership (Sep 16, 2008)
 
 
NEC Electronics America Hires 60 New Employees to Support Expanded Semiconductor Manufacturing Capabilities (Feb 6, 2007)
 
 
See more manufacturing news.
 



Documentation