Beginning of this page
Jump to main content

Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.


The following page content corresponds to the products formerly marketed by NEC Electronics

Channel Decoder




Overview

NEC Electronics' COFDM devices are commonly used in Terrestrial STB, IDTV and digital/hybrid DVD Recorders. This high-performance COFDM demodulation LSI can be connected effortlessly with a tuner and a MPEG for digital terrestrial handling. NEC Electronics' expertise on this front is recognized and proven in the DVB-T market in Europe.

Product Lineup

Product Lineup uPD61540 DVB-T COFDM Europe etc, uPD61541 DVB-T COFDM Europe etc,


Product List

Features Product
µPD61540 µPD61541
Development Status Sample
MP
Function Transport Stream 2 Systems 2 Systems
C/N Output
TS-Output Mask
Equalizer
RF (tuner) interface Low IF, I/Q Low IF
Nordig Unified 1.03-compliant -


Status: =Mass Production, =Under Offer, =Under Development, -= Under Planning
Function: =Support, -=Not support
SDK: Software Development Kit



Inquiry Concerning Digital AV LSI